Altium Reporting Options

File in Previous Format

Date : 3/14/2014
Time : 10:00:33 AM
Filename : C:\DXP_Projects\THS6226 REV.A\THS6226RHB.PcbDoc

Version Warning
6.3 CAUTION - Via connections to both hatched and solid signal layer polygons are now controlled by the polygon connect style rule. Re-pouring polygons may result in physical copper differences.
Summer 09 CAUTION - File contains old violation objects. These violations are no longer supported & will not be loaded. Please run DRC after opening this file in order to refresh the violations.
Summer 09 CAUTION - Existing testpoint rules and settings are used as fabrication testpoint information.
Altium Designer update 19 CAUTION - Air Gap Width attribute was introduced to Polygon Connect Style Rule. Air Gap Width attribute now controls the distance between poured polygon and pads on the same net - this value was previosuly taken from clearance rule while ignoring net subscope leading to sometime unexpected results.


This file was generated by an earlier version of the software